AXIS#.MT.DISALLOWINTERRUPT

Description

This parameter sets the motion task control word specifying whether or not to be able to interrupt the current motion task.

It takes the following values:

Value Description
0 Allow Interrupt
1 Disallow Interrupt

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL.

Code

MT.DISALLOWINTERRUPT Will configure Motion Task 0 to disallow being interrupted.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write Array
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  
Start Version  

Stored in Non-Volatile Memory

No

Variants Supported

Supported on all drives.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MT.DISALLOWINTERRUPT

6314

18AA

Unsigned8[32]

Read/Write

-

AXIS2.MT.DISALLOWINTERRUPT

71850

118A

Unsigned8[32]

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MT.DISALLOWINTERRUPT

6314

Unsigned8[32]

Read/Write

-